8/18/2019 7:10 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear mesowball, I attached the solution here. See attached. 1. Open@pcs7typicalsAPLV8 in GraCS 2. Copy the block icon you want to new pdl 3. Customized Object ->Edit 4. Separate the block icon, look for symbol 5. Open Configuration dialog -> assign pictures 6. Choose the pictures (Working With WinCC V7.5) Section 3.8.7.19 Extended Status Display 7. Arrange the block icon and finish editing 8. Change the Variant for automatic block creation 9. Create a customized @pcs7typicals to store your customized block icon. 10. Change the block icon number assignment in CFC block properties Added an extra guide for customization on .emf file. You may you Microsoft Power point, Microsoft Visio, Graphic design, Paint to create your emf file. Hope this is helpful for you. AttachmentHow To Change Standard Block Icon Picture.pdf (57 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
8/18/2019 6:10 PM | |
Joined: 8/22/2018 Last visit: 3/2/2021 Posts: 35 Rating: (0) |
Hi Jaz, thank you very much. I will try it out many thanks snowball |
8/19/2019 9:44 AM | |
Joined: 3/13/2015 Last visit: 8/27/2024 Posts: 136 Rating: (39) |
Hi, Please take a look add the custom picture directory option in the block icon properties. This way you just have to configure your block icon instead of modifying it. See for more information: https://support.industry.siemens.com/cs/ww/en/view/109760968/115421623307 Regards, |
Last edited by: Molthoff at: 08/19/2019 09:49:47 |
|
Follow us on