8/31/2013 7:36 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, It could be that the "new" battery's were not so new You can try to do the depasivation thing again and measure the voltage at the poles. If the voltage is o.k. check the poles at the battery compartiment, they might have bin oxidated. Clean them, if all o.k. and still problems, powersupply is dammaged.. You can try with new power supply if you have one spare. Note, there is the possibility to put a backup battery at the CPU direct, there is a connector to do so. regards, Marcjan Attachmentext-bat.pdf (839 Downloads) |
Last edited by: Marcjan at: 8/31/2013 7:47 PMProblem solved? |
|
This contribution was helpful to1 thankful Users |
9/8/2015 9:51 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Jhon Alvati is split to a separate thread with the subject Changing PLC battery questions. Best regards |
10/27/2015 10:25 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Jhon Alvati is split to a separate thread with the subject Changing the battery. Best regards |
Follow us on