7/17/2019 9:44 PM | |
Joined: 12/18/2014 Last visit: 8/31/2024 Posts: 33653 Rating:
|
Write from the HMI into a parameter e.g. V1 of a mathematic instruction via Parameter-VM-Mapping. |
7/17/2019 10:13 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating:
|
now I struggling which element I should use in TIA portal to change analog value ? I/O field? |
7/18/2019 4:01 AM | |
Joined: 12/18/2014 Last visit: 8/31/2024 Posts: 33653 Rating:
|
Attached are the TIA project, the LOGO! program and screenshots. Unfortunately I only have TIA V15.1. But the screenshots should help. In TIA use a I/O filed. In LOGO! program use a mathematic instrution and Parameter VM Mapping. AttachmentForum.zip (258 Downloads) |
7/22/2019 7:04 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating:
|
Dear Ixo, Lets say that I want to steer a % of valve open via hmi screen. I suppose that the analog output in Logo analog extention module should be connected to this valve. Where is analog output block in your program Ixo ? Attachmentvalve Runtime_mit_LOGO!8.FS4.zip (234 Downloads) |
7/22/2019 7:47 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating:
|
Do you think this (attachment) would work ?
Attachmentvalve Runtime_mit_LOGO!8.FS4.zip (208 Downloads) |
Follow us on