7/16/2021 12:35 PM | |
Joined: 4/28/2015 Last visit: 12/4/2023 Posts: 3294 Rating:
|
Hi, sorry, but I can't read anything on your picture. The u-boot shell is only accessible via UART cable. You need to get the file fw_env.config (from here) and copy it to /etc in order to change the boot order from the running system. Unfortunately this file is missing in Industrial OS, but available in Example Image. After having the file copied you can change the boot-order with
These changes are persistent automatically. Best regards! |
Follow us on