3/13/2015 10:55 AM | |
Posts: 1 Rating: (0) |
Hello All, this is my first post so bare with me after changing the cpu . the connections were deleted so i reconfigured them. attached is a screen shot of the two project windows. hope i have explained my first post well enough! *fingers crossed* Attachmentscrnshot.docx (129 Downloads) |
3/13/2015 7:53 PM | |
Posts: 167 Rating: (4) |
Hi It would be better if you can put a screen shot of HW Config or network view of your system. Regards, poya |
Follow us on