3/11/2021 9:13 AM | |
Joined: 2/25/2021 Last visit: 11/2/2022 Posts: 73 Rating: (0) |
Here you have it! Vinha_1Cuba represents LOGO1, and Vinha_2Cuba represents LOGO2. Both programs are in LAD. I also added the network to the .zip file, with both programs in FBD. I have no idea why LOGO 2 isn't recognizing the information from LOGO 1. EDIT: I hadn't updated the network, it had some errors. Now it should be correct, but still not working as desired. AttachmentLOGO1+LOGO2+NETWORK.zip (238 Downloads) |
Last edited by: GCosta at: 03/11/2021 09:37:39 |
|
3/11/2021 9:37 AM | |
Joined: 12/18/2014 Last visit: 5/23/2024 Posts: 33099 Rating: (4085)
|
With LAD diagrams you can't create a network project. I have in both LOGO!s the connection inserted. In the connection table of the client (LOGO_1) I have entered the corresponding bytes (VB4-VB7). AttachmentTest.zip (234 Downloads) |
This contribution was helpful to1 thankful Users |
3/11/2021 10:38 AM | |
Joined: 2/25/2021 Last visit: 11/2/2022 Posts: 73 Rating: (0) |
Many thanks, everything is working fine now |
This contribution was helpful to1 thankful Users |
3/11/2021 10:46 AM | |
Joined: 12/18/2014 Last visit: 5/23/2024 Posts: 33099 Rating: (4085)
|
Hello GCosta, you're welcome. |