3/1/2016 9:53 PM | |
Joined: 8/31/2013 Last visit: 5/26/2024 Posts: 607 Rating:
|
Hello Could you check your Lic of OS or ES which you have used ? |
Warm Regards |
|
3/1/2016 11:29 PM | |
Joined: 3/14/2008 Last visit: 8/30/2024 Posts: 2093 Rating:
|
Hi, that is the disadvantage you have when working with workgroups. Changing a user, adding a user and changing passwords have to be done at all PC stations and in the multi-project. When you configure the PC stations in a domain, you can do this centrally, or by using Simatic Logon. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
12/21/2017 9:02 AM | |
Posts: 2 Rating:
|
Before you change your password, there are two things you need to do.First, reset all passwords and, second, close the other accounts that don't need to change your password |
Last edited by: Ramkerty at: 12/23/2017 4:20:17 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on