11/18/2020 3:47 PM | |
Joined: 4/11/2016 Last visit: 6/24/2024 Posts: 3 Rating: (0) |
Hi everyone, I am looking for "wire break" diagnostic of inputs connected to a DI module, specifically 6ES7131-6BH01-0BA0 https://mall.industry.siemens.com/mall/en/WW/Catalog/Product/6ES7131-6BH01-0BA0 The module manual clearly states that the module is capable of doing such diagnostic in chapter 5.2. "Diagnostics interrupts The module generates a diagnostic interrupt at the following events: ● Wire break ● Parameter assignment error ● Supply voltage missing" However, in the manual there is no information about evaluating HW interrupts created by singular DI. On the other hand, manuals of HF DI modules have a specific chapter, where such information is available. My question as follows, the "wire break" diagnostic for DI module 6ES7131-6BH01-0BA0 is referred to a cumulative "wire break" diagnostic of all DI channels present in the module, or there is a possibility to do a diagnosis for each channel separately? I found a system diagnostic FAQ https://support.industry.siemens.com/cs/ww/en/view/68011497 but there is no example of DI module's channel diagnosis. The instruction GET_DIAG retrieves just diagnostic information about a module and it's submodules, so I was wondering if there is an instruction which is able to retrieve channel specific diagnosis? Thank you. |
Last edited by: Jen_Moderator at: 11/19/2020 09:15:16Optimized link. |
|
11/18/2020 5:03 PM | |
Joined: 7/7/2010 Last visit: 7/12/2024 Posts: 14948 Rating: (2393) |
https://support.industry.siemens.com/tf//ww/en/posts/et200sp-diagnostic-alarm-how-to/196921 may help. Someone found changing the hardware configuration to enable more diagnostics information solved their particular problem with wire break diagnostics.
|
science guy |
|
11/20/2020 9:27 AM | |
Joined: 4/11/2016 Last visit: 6/24/2024 Posts: 3 Rating: (0) |
Thanks for your replies guys. I have found a TIA Portal project which has channel diagnostics implemented. https://support.industry.siemens.com/cs/ww/en/view/109480387 |
Last edited by: Jen_Moderator at: 11/20/2020 12:23:53Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on