4/28/2016 2:18 PM | |
Posts: 4 Rating: (0) |
Hi, I have Single Motor Module 6SL3120-1TE13-0AA3, Which trips off and I have to reset it by switching off the Mains. Can anyone help me how do I check the fault code so I know what is the problem due to which it is tripping off? thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/29/2016 2:54:47 PMNew subject after splitting |
|
4/30/2016 11:35 AM | |
Posts: 251 Rating: (11) |
hello, which control unit and version do u use ? |
4/30/2016 12:20 PM | |
Posts: 1529 Rating: (202) |
Assuming the webserver has been enabled and the defaults have not been changed.... Plug in an Ethernet cable to X127 and go to http://169.254.11.22 with any browser to go to the drive internal webpage. You can find the diagnostic logs there. |
This contribution was helpful to1 thankful Users |
5/19/2016 11:13 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878) |
Which is drive? Infeed module? Which is CU unit? What is control mode type? |
8/31/2016 12:18 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by FranMar is split to a separate thread with the subject How can i connect 6SL3120-1TE28-5AA3 with starter ?. Best regards |
Follow us on