4/25/2016 9:42 AM | |
Joined: 11/18/2015 Last visit: 5/23/2024 Posts: 87 Rating: (1) |
Hello, It looks the same in V6 only without the signs. See attached screenshot. We are using PCS7 8.1 SP1. Regards, Tomact |
4/25/2016 12:50 PM | |
Joined: 11/18/2015 Last visit: 5/23/2024 Posts: 87 Rating: (1) |
Hello,
Regards. |
4/25/2016 1:12 PM | |
Posts: 75 Rating: (18) |
Hello Tomact, what's the value of the tooltip text in CS? |
This contribution was helpful to1 thankful Users |
4/25/2016 4:54 PM | |
Posts: 75 Rating: (18) |
Since the weird chars are also available in CS I agree with you that this is probably a migration issue. You migrated from PCS7 V6.1 to PCS7 V8.1: that means you migrated from WinCC V6.0SP3 to WinCC V7.3. With WinCC V7.2 WinCC introduced Unicode and such weird chars were often Unicode issues. How did you migrate? Did you migrate in one step? It seems that WinCC V7.3 only supports migration from WinCC V6.2.3 or higher (see chapter 5.3 Conditions for Migration in WinCC V7.3: General information and installation). Link for download is WinCC V7.3 - General information and Installation |
This contribution was helpful to1 thankful Users |
Follow us on