3/18/2016 2:32 PM | |
Joined: 11/17/2010 Last visit: 9/12/2024 Posts: 216 Rating: (40) |
Hi, I tried to write an example in the doc attached.
1st network : initialize Pump Index and Temporary Time comparison. 2nd network : Compare only pump not sarted. (It would be better to compare with function "less or equal" instead of "less" 3rd network : Start the pump that have the less running time. Hope there is no error and this is what you want. Regards. AttachmentChoose pump to start (Ladder).docx (94 Downloads) |
Last edited by: Panov69 at: 3/18/2016 2:33:24 PMLast edited by: Panov69 at: 3/18/2016 2:33:34 PM |
|
This contribution was helpful to1 thankful Users |
3/21/2016 9:54 AM | |
Posts: 22 Rating: (0) |
tanks for the reply, This solves the problem :) |
This contribution was helpful to1 thankful Users |
Follow us on