12/4/2022 3:15 PM | |
Joined: 3/14/2020 Last visit: 8/29/2024 Posts: 7 Rating: (0) |
Hello, I am suffering a lot with this CIM module, even though I should be able to solve a simple task with it. The CIM module should read a couple of analog and static (digital and merker) states, based on which it should send an SMS message. Also, based on the received SMS, you should send a couple of analog values in response. I have attached the sample program and the CIM module config file, I have created a short text (editable) document. The CIM module should read some data from LOGO! via the Modbus TCP protocol. The CIM module is functional and has a connection with Logo!. It send SMS by power on/off. I'm doing something very wrong, please look at my attachment and if anyone can help me effectively, I thank you in advance. Best regards, ------------------------------------------------------------------------------------------ AttachmentSiemens_CIM_set_basics.zip (578 Downloads) |
Last edited by: Jen_Moderator at: 12/05/2022 05:18:13New subject after splitting |
|
12/4/2022 3:56 PM | |
Joined: 3/14/2020 Last visit: 8/29/2024 Posts: 7 Rating: (0) |
Hi, Yes... |
12/4/2022 4:02 PM | |
Joined: 12/18/2014 Last visit: 10/16/2024 Posts: 33968 Rating: (4223)
|
Why do you use the Modbus connection instead of the S7 connection? |
12/4/2022 4:53 PM | |
Joined: 3/14/2020 Last visit: 8/29/2024 Posts: 7 Rating: (0) |
I was try this way... If somebody show me the S7, how to - I will made with it... Just like to reach the functionality |
12/5/2022 3:19 AM | |
Joined: 12/18/2014 Last visit: 10/16/2024 Posts: 33968 Rating: (4223)
|
I would recommend you: Start a Support Request. Edit: I find it sad that Siemens is offering such a device for sale and all you can find on the Siemens websites is a poorly written manual. Siemens should create practical application examples for this. |
Last edited by: ixo65 at: 12/05/2022 03:24:07 |
|
This contribution was helpful to2 thankful Users |
12/5/2022 8:43 AM | |
Joined: 3/14/2020 Last visit: 8/29/2024 Posts: 7 Rating: (0) |
I was now ask for it - hope I will get usefull and helpfull information - after that I will share with you folks! |
Follow us on