12/31/2015 12:05 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, These outputs can be used in a so called 3 step controller: This has nothing to do with a true "step motor" that is used for positioning. Could you be more specific on the "step motor" you want to use? |
Last edited by: jklm at: 12/31/2015 12:47:38 PMBest regards |
|
1/3/2016 10:50 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, It also works with two outputs with opening pulses and closing pulses. You than call the FC1 in a time triggered OB (OB35). To be tested ... AttachmentFB42.pdf (214 Downloads) |
Best regards |
|
Follow us on