1/27/2017 1:20 PM | |
Joined: 11/19/2016 Last visit: 10/19/2024 Posts: 36 Rating: (0) |
Hi, I have used CM1241 (RS485) Module to communicate with HMI for through Modbus. but now for the same PLC I want to communicate with DCS which is having same RS 485 Communication protocal. What I have to do for establishing communication between PLC and DCS. DCS will only monitor PLC Values. Can I use one more CM1241 in the same PLC and configure that for communicating with DCS?? Will it support 2 RS 485 Modules ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/27/2017 3:29:31 PMNew subject after splitting |
|
1/28/2017 7:02 AM | |
Joined: 11/19/2016 Last visit: 10/19/2024 Posts: 36 Rating: (0) |
Thank you.. for support... Vinayak Parab |
Follow us on