10/11/2020 1:26 AM | |
Joined: 8/15/2015 Last visit: 8/21/2024 Posts: 133 Rating: (4) |
Dear All , so I managed to make it work https://support.industry.siemens.com/tf/ww/en/posts/how-to-reset-network-input-in-logo-8-fbd-program/142779 "V_pulse.zip" So in order to trigger the SMS : Here I attach a picture of how this is done , depending on how you want to play it you can use an on-delay or off delay depending on your needs the way is set up is always the same Then you setup the actions and signals and events to send out the SMS with your whatever you need in my case a status SMS that shows all details of all the inputs only when that NI or NQ is high |
Follow us on