7/10/2016 9:03 AM | |
Joined: 12/18/2014 Last visit: 7/22/2024 Posts: 33386 Rating:
|
The logo has the net class C. Thus are the IP addresses in the range of 192.0.0.0 to 223.255.255.255, the subnet mask is 255.255.255.0.
PC = 192.168.178.NNN Now I have changed to test the IP address to 192.168.078.030. The Logo software notes the transmission attempt that the logo is in a different subnet as the PC and proposes to create an additional, temporary Ip address for the PC. If you confirm the proposal with Yes, this temporary IP address is created for the PC and the Logo software can communicate with the logo and the program can be transferred. This is clearly the indication that the logo can not communicate with other devices, which are in a different subnet. AttachmentTest.wmv (122 Downloads) |
Follow us on