9/24/2018 9:25 AM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33840 Rating: (4206)
|
In attachment is what to do on LOGO! side |
This contribution was helpful to1 thankful Users |
9/24/2018 10:54 AM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating: (1) |
Ok I will try to add this on logo. what string text command to write on cmr? |
9/24/2018 11:08 AM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33840 Rating: (4206)
|
Which Firmware has your CMR? The last, V2.1.5? |
9/24/2018 1:44 PM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33840 Rating: (4206)
|
Firmware update V2.1.5 for LOGO! CMR2020 (6GK7142-7BX00-0AX0) and LOGO! CMR2040 (6GK7142-7EX00-0AX0) Look at yourself ... <Passwort>;LOGO=VM0.0,1,BIT |
9/24/2018 2:57 PM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33840 Rating: (4206)
|
Did you set up everything necessary to send Alias SMS?
AttachmentUntitled.pdf (234 Downloads) |
This contribution was helpful to1 thankful Users |
9/24/2018 6:35 PM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33840 Rating: (4206)
|
Sounds good that it works now. |
Follow us on