4/15/2020 8:44 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, Good that you found the BPCM library. This library gives you a good impression of the CMT's. It's basically a newer and better way of the Process Tag Types. A CMT consists of a few blocks like a VlvL with two digital input drivers and an output driver. You can use the technology editor to drag block parameters so that they can be used in Plant Automation Accelerator for example (to do bulk engineering). A few good documents are listed below: Synchronization of Control Module Types Equipment Modules for the Chemical Industry |
Last edited by: Oreca at: 04/15/2020 08:47:38If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on