Industry Online Support
Technical Forum
4/23/2012 5:57 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hello, with the LOGO! series 0BA6 and 0BA7 it is possible now to calculate lineare functions (with block amplifiver) and polynoms as funtion of an analog value Ax (wilock Math. function). It is helpful to use MS-EXEL to calculate the coefficients of a polynome with order 1 (linear) or up to 4 or 5. This coefficients are the basic to define the Parameters for a LOGO! circuit witch then can calculate a polynom (most as approximation for the real data). Here is the link to that tool: EXCEL tool polynom regression for linear and nonlinear calculations The calculations i have done here to solve the question aremuch easier with this tool... Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on