7/26/2019 11:50 AM | |
Posts: 5 Rating:
|
Hi dear, can you help me with a question please? I'm using 2 cu with a PLC, everything was ok. Each with an IP address. But now it has stopped. I formatted the memory card of the both cu and recorded the project again through the starter (offline). But the COM led of the two CUs are still on. Can it be topology error? I already checked the IP address. *The project was made with starter version v4.4 and I'm using the last one. Thanks. Rainerio ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/26/2019 13:22:00New subject after splitting |
|
8/1/2019 12:13 AM | |
Posts: 5 Rating:
|
How can I configure the topology on CU305 PN? I can't find drive-cliq. *Attached is the error image. *I have two CUs connected with a PLC. Please. Rainerio |
8/1/2019 12:26 PM | |
Posts: 5 Rating:
|
Hi, I dont have TIA installed on my PC. I'm trying to configure with STARTER by Ethernet. In the messages shows this error: A08526 (F): PROFINET: No cyclic connection. I think my problem is like this video: https://www.youtube.com/watch?v=3YyyWOv7MJA But my model is S110 CU305 and not G120. Help me please! Thank you. |
Last edited by: Jen_Moderator at: 08/01/2019 12:56:34Embedded Video. |
|
8/1/2019 1:30 PM | |
Posts: 5 Rating:
|
Ok, thank you I gonna check it and came back here! |
8/4/2019 2:20 PM | |
Posts: 5 Rating:
|
Thank you gentlemen, I got it. |
This contribution was helpful to
1 thankful Users |
Follow us on