8/17/2008 1:51 AM | |
Joined: 6/14/2008 Last visit: 1/25/2022 Posts: 65 Rating: (3) |
HI!! I want to connect with "S5 95U DP master" by "COM PROFUBUS V5.1.2.3" using "PC ADAPTER USB 6ES7972-0CB20-0XA0." On the screen of "Set PG / PC Interface", it is displayed as "None" and there was no "PC Adapter." Please see the appended PDF file. What does my setup lack? I am using this "PC ADAPTER USB 6ES7972-0CB20-0XA0" satisfactory in "SIMATIC Manager." Attachmentmelsec profi.pdf (669 Downloads) |
Follow us on