6/4/2018 11:54 AM | |
Posts: 6 Rating: (0) |
Hello, Is it possible to use Brother QL-800D printer with Comfort Panels? Siemens provides driver for the older model QL-650D, so are they compatible? |
11/19/2018 1:25 PM | |
Joined: 3/28/2017 Last visit: 4/22/2024 Posts: 2 Rating: (0) |
I tried to write barcode via brother QL-650TD printer with TP900 comfort panel and works together succesfully. You can find the result is in the attached photo.Barcode useful for scanner.Also barcode font 21 in attachment photo.I tried to write bigger font and I got more succesfully results. Steps this application; 1-Download brother QL-650TD driver from siemens support.Link below https://support.industry.siemens.com/cs/us/en/view/11376409 2-Install driver to comfort panel via Prosave 3-After installed the driver, select the label size from the DKRoll application that occurred on the panel desktop.I selected Continous paper size choice.If you want you can select autocut choice 4-Last step write barcode |
Last edited by: Jen_Moderator at: 11/20/2018 7:31:42 AMOptimized link. |
|
Follow us on