3/21/2023 5:16 PM | |
Joined: 1/21/2013 Last visit: 12/20/2024 Posts: 3396 Rating: (530) |
Hi christopherreyes, Did the time synchronization with the NTP server work before? I mean, was the time synchronized? The only thing I can think of is that the settings are reset on startup if there are errors. But maybe it's a hardware failure. You should contact support for that. As for the trace forwarder settings, do not worry. They are disabled on reboot for security reasons. Kind regards |
Follow us on