3/26/2008 6:38 PM | |
Posts: 102 Rating: (1) |
Dear Experts, I have made one sample program using STRUC L 4.2.7 In my programe I have included following hardware PM16, MS41, SS1(X01), SS1(X02) I have intialised @DU3 block in SEND FP. After compliing and burning the EPROM when I start PM16 it will give me error Flashing "C" on 7 segment LED display of PM16. Can u look into my program and tell me where I m doing mistake? I m attaching the program here. with regards, Dutta AttachmentPRJ06.zip (446 Downloads) |
3/28/2008 10:28 AM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
I think the @DU1 (DUST1) block is missing, add it to FP-@P4SEK and connect it to D01_P1.X01, sorry I forgot it yesterday. Due you have a SS1 in Port1, you needa PG (with 20mA) or a TTY/RS232 converter. Please let the IBS-Tool run under DOS, see this notes. |
|
|
4/1/2008 11:03 PM | |
Posts: 102 Rating: (1) |
Dear Experts, I have got two SS1 Hybrid modules and I have placed them on PM16 at X51 and X52 sockets But now when I power on the rack it gives me error on PM16 like Slowly Flashing "b" what does this error means. I m also attaching the program code with this mail. Please have a look and reply me. I m also not able to diagnose with IBA 5.01 please help me. dutta AttachmentMYNE1.zip (458 Downloads) |
9/10/2008 10:15 PM | |
Posts: 75 Rating: (13) |
The flashing "b" means, that the battery in your rack is empty or not existing. It is the same battery like in S5. |
9/15/2008 4:42 PM | |
Posts: 75 Rating: (13) |
Is there any other reason for a flashing "b" ? regards Pasman |
Follow us on