2/27/2020 6:29 AM | |
Joined: 4/13/2017 Last visit: 2/19/2022 Posts: 2 Rating: (0) |
Requesting help configuring command variable on SICAM 230 v 6.51. It appears that the SICAM IEC61850 driver does not correctly identify the variable path for a IEC61850 breaker command variable. eg. Actual Patch CSWI.Pos.Oper.ctlVal is instead identified as CSWI.Pos.ctlVal, when importing variables from CID. Is this the correct behaviour ? Also please explain the correct CDC / data type / expected settings to correctly configure a switching object command variable in this case. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/27/2020 14:29:07New subject after splitting |
|
Follow us on