11/7/2022 8:45 AM | |
Joined: 3/2/2007 Last visit: 5/8/2024 Posts: 929 Rating: (5) |
Kindly, do you have an idea on how to commission the below two cards, installed on a Simoreg K dc drive ? 6RA8232-1KB0, supplem.board Z1011 F.6RA22 MP SINEC-L1 and DUST 6 interface without mounting set 6RA8232-1VB0-0 , Simoreg option module Z1022 , supplem.board Z1022 F.6RA22 MP higher-level PID controller enhanced version with mounting set 6RA2232-6DV62-0, Simoreg K converter with microprocessor for four-quadrant drives connection (B6)A(B6)C, 3-phase, AC 380V controllable field rectifier D400/130 MREQ-GDG 6V62 |
Last edited by: Ziemens at: 11/07/2022 08:46:27... thank you ... |
|
Follow us on