5/27/2023 12:43 PM | |
Joined: 12/15/2022 Last visit: 3/16/2024 Posts: 1 Rating: (0) |
Hi there, I’m trying commissioning a sinamics drive G130 CU320-2 PN with a terminal module TM31 who’s got all the digital inputs for commanding the drive wired to it using the STARTER software V5.4.2.1. The problem is when i try to start the motor, i got the following: [42] Switching on inhibited - set "OC/OFF2" = 1 (p0844, p0845) The diagnostic buffer only shows a warning 1073: POWER ON required for backup cpoy on memory card, i powered off/on the control unit but nothing happened. thanks to you all ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/30/2023 09:28:39New subject after splitting |
|