8/12/2014 4:13 PM | |
Posts: 247 Rating: (2) |
available devices missing CU250s |
8/12/2014 5:16 PM | |
Posts: 247 Rating: (2) |
Thanks dearChristoph :) |
5/30/2015 5:07 PM | |
Posts: 1 Rating: (0) |
I am following the same path, but still cannot configure the drive. Using V4.4 STARTER with added SSP's. Can find with accesable nodes via USB & uploadc, or create offline with same error message when I try to configure: "HW Coonfig cannot be opened" and "The device is not part of a STEP7 station or the HW configuration is unknown" (see attached) Any Suggestions? AttachmentAttempting to comission a new G120 with CU250S.doc (264 Downloads) |
Follow us on