6/29/2017 8:57 AM | |
Posts: 9 Rating: (0) |
Hi friends I want to communicate one master and four slave CPU of 1214c ac/dc/relay type (all CPU are of same type) and i have done with the communication between two CPU but third one is not communication properly so kindly suggest me the sample program for this thanks & regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/30/2017 10:02:58 AMNew subject after splitting |
|
6/30/2017 12:21 PM | |
Posts: 9 Rating: (0) |
sir CPU is 1214c ac/dc/relay communication is by siemens green TCP/IP cable all CPU are of same type modle number is 6ES7-214-1BG40-0XB0 |
6/30/2017 12:46 PM | |
Posts: 9 Rating: (0) |
sir, I have tried it with GET/PUT as well as TSEND_C/ TRCV_C it is helpful only for communication between two CPU |
6/30/2017 1:01 PM | |
Posts: 9 Rating: (0) |
Yes i am using siemens green TCP/IP (profinet) cable |
6/30/2017 2:51 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi abdul, try this: Configuration and application of PROFINET I-Device function this would be the easiest way to communicate whit the requirements you have. hope this helps, regards, |
FCK WAR! |
|
7/1/2017 7:26 AM | |
Posts: 9 Rating: (0) |
Sir, kindly send me the sample program for that if possible |
Follow us on