9/21/2020 6:08 AM | |
Posts: 3 Rating: (0) |
Hi, I want to establish communication betweek siemens s7-1200 PLC and a nvidia jetson nano device using PROFINET. How do I find a GSD file for this application? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/21/2020 11:50:14New subject after splitting |
|
9/21/2020 6:11 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
since the nvidia doesn't support PROFINET there is no GSDML file for it. |
9/21/2020 11:43 AM | |
Posts: 3 Rating: (0) |
Is there any other way to communicate with NVIDIA jetson nano? |
9/21/2020 11:47 AM | |
Posts: 3 Rating: (0) |
OS on the nano is Ubuntu and going to use Python to develop the application |
9/21/2020 12:04 PM | |
Joined: 3/30/2020 Last visit: 4/28/2024 Posts: 4459 Rating: (931) |
Using Ethernet communication is the best option. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on