4/19/2024 9:34 AM | |
Joined: 1/9/2024 Last visit: 6/4/2024 Posts: 1 Rating: (0) |
Hello! I have a similar situation going on here, where need to communicate with a different PLC on a different project & network. Correct me if I am wrong, but all you need to do is add PN/PN coupler, configure your side of the coupler (mine is X2), insert GSD file of other PLC and connect it to other side of the coupler (X1), and as for PN/PN coupler configuration for the other port X1 configuration specify access as "Outside of project" Kind of like in the photo. Transfer areas from my PLC are configured in connected port device, and transfer areas from PLC of other project are configured in port device that's not connected to anything. Thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_2720835 at: 04/19/2024 09:59:52Last edited by: Jen_Moderator at: 04/22/2024 06:28:32New subject after splitting |
|