3/25/2019 9:18 PM | |
Posts: 6 Rating: (0) |
Hey, I'm kinda of new to this whole ethernet Profinet. I have got the device configured on the TIA v15.1 and download to the PLC. But I am a little lost on what tiggers the output to the scanner to turn on it and off. I am also a little lost on how to read the inputs from the scanner. I did follow these instructions sick gave me. That are linked below. Hardware: plc-s7-1515-2 barcode scanner sick clv630-6120. Software is siemens TIA V15.1 AttachmentProfinet Setup with SICK(1)-compressed.pdf (620 Downloads) |
3/27/2019 5:20 PM | |
Posts: 6 Rating: (0) |
Got it figured out .Q needed to be a 1.0 and the ibxx was 2-33. Now just got to get it to send to a server |
3/27/2019 7:05 PM | |
Posts: 6 Rating: (0) |
Can anybody help me turn this into data that I can send to a server I'm a little lost |
Follow us on