8/8/2014 11:11 AM | |
Posts: 1368 Rating:
|
Hi, have a look here: AG_SEND for S7-300: http://support.automation.siemens.com/WW/view/en/17853532 AG_SEND for S7-400: http://support.automation.siemens.com/WW/view/en/24693800 and here http://support.automation.siemens.com/WW/view/de/47885244 |
Last edited by: Pittiplatsch at: 8/8/2014 11:12 AM |
|
8/8/2014 12:09 PM | |
Joined: 2/19/2013 Last visit: 11/10/2024 Posts: 185 Rating:
|
I allreay read this manuals, but it´s a little unclear. For the CPU 414 it needs the use of the AGSEND, but for the CPU 317 it needs the use of the TSEND instruction, as it has integrated PN port. I will upload my project to see if something´s misssing.
AttachmentCom_400_.zip (49 Downloads) |
8/8/2014 12:48 PM | |
Posts: 1368 Rating:
|
You are right, with a S7-300 PN-CPU, you use the TCON, TSEND and TDISCON. Then this FAQ is relevant for you http://support.automation.siemens.com/WW/view/de/29737976 Can you post only a screenshot from your AGSEND-CALL, TCON_Param and TADDR_Param? Thx |
8/11/2014 8:32 AM | |
Joined: 2/19/2013 Last visit: 11/10/2024 Posts: 185 Rating:
|
That is the problem. I don´t know how to change these parameters and with which value do I have to repcae them. |
8/11/2014 8:50 AM | |
Posts: 1368 Rating:
|
can you post the TCON_PARAM in "online view"? And the AG_SEND configuration on other side! |
Follow us on