6/28/2010 12:17 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Grim Reaper, As from S7-PLCSIM V5.4 + SP3 you can use S7-PLCSIM to simulate multiple CPU modules simultaneously in a STEP 7 project and establish communication between the CPU modules. The following communication blocks are supported for communication:
& Here you will find Which components are not supported by S7-PLCSIM V5.4 SP3? |
Last edited by: Ammy at: 6/28/2010 12:19 PMAmmy |
|
6/28/2010 1:41 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
How do you simulate communication between two CPU modules?
|
9/13/2017 10:37 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by AutoGen_107316 is split to a separate thread with the subject Trying to communicate between two PLC using simulation - Data is not getting transferred. Best regards |
Follow us on