3/21/2016 5:57 AM | |
Posts: 30 Rating:
|
Hi, I have two different PCS7 project. Both project have S7-415H CPU but I have only one of them is CP-443, Can i communicate between the two CPU using the Ethernet port on the CPU itself. Please note both CPU are having communication connection with respective Winncc servers. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/22/2016 12:37:16 PMNew subject after splitting |
|
3/22/2016 8:44 AM | |
Posts: 567 Rating:
|
Hi, have a look at the following FAQs: |
Follow us on