3/21/2019 3:20 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi, 1. just take a S7-connection. 2. "Unknown" is right. it´s called a unspecific connection, that means the communication partner is not part of this projekt. As you have a S7-1500, it can´t be projected in S7 classic. 3. normally you just need to establish the connection on one side. the CPU on this side just accesses the other CPU with PUT and GET blocks. In S7-1500 CPU you need to allow the access for PUT/GET in CPU-properties in "Protection&Security" Also this FAQ can help you: Sample Program: S7 Communication with blocks FB14 ("GET") und FB15 ("PUT") of the CPU 317-2PN/DP hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
3/22/2019 7:14 AM | |
Joined: 1/22/2018 Last visit: 4/15/2024 Posts: 5 Rating: (1) |
It worked, thank you. |
Follow us on