5/9/2017 11:19 AM | |
Joined: 11/4/2015 Last visit: 8/28/2022 Posts: 6 Rating:
|
Dear experts; I have facing problem with the communication between s7 315-2 PN/DP with S120 using Profinet. My devices are …. CPU IP: 192.168.0.1. & CU320 IP : for X150 P1 is 192.168.0.15. Smart line module , double motor module and one servo motor. My main problem is that there is a SF & BF fault in s7 hardware and it shows that no S 120 hardware is found. I sent you the picture for that . please give me solution for that. I am new in s120 system. If it is possible then give me the procedure for communicating s7 300 & s120 using profinet------------------------------------------------------------------------------------------ AttachmentPictures.zip (91 Downloads) |
Last edited by: Min_Moderator at: 5/9/2017 4:03:19 PMNew subject after splitting |
|
5/9/2017 12:31 PM | |
Joined: 11/4/2015 Last visit: 8/28/2022 Posts: 6 Rating:
|
Dear Expert; I am using double motor module but connect only one motor . is there any problem for that? |
5/9/2017 12:33 PM | |
Joined: 5/12/2006 Last visit: 3/30/2023 Posts: 21352 Rating:
|
no |
5/13/2017 1:50 PM | |
Joined: 11/4/2015 Last visit: 8/28/2022 Posts: 6 Rating:
|
Problem solved by reset the whole system and re configuring. |
Follow us on