4/23/2019 12:33 PM | |
Posts: 76 Rating:
|
Hello engineers, I have configured S7-Connection between S7-400 and ET200SP by following these instructions: How do you configure and program an S7 connection and the FB15 "PUT" and FB14 "GET" function blocks for data transfer between an S7-1200 CPU and an S7-300 CPU? When I tried to run a simple test, I got: Error = 1 and Status = 1. By reading help of the GET function, I got to know that this is referred to communication problems i.e. - Connection description not loaded (local or remote) - Connection interrupted (cable, CPU off, CP in STOP mode) - Connection to partner not yet established - FB cannot run on an S7-400 CPU In the Standard Library -> Communication blocks -> FB14 "GET" and FB15 "PUT" I can see under "Family" column that it states "CPU_300", but I didn't find any other GET or PUT blocks in the Communication blocks folder. I have defined CPU 416-2 DP station in the hardware configuration. QUESTIONS: *** Where to find these blocks for 400 CPUs, because obviously this could be a source of problem? *** Is it possible to test this kind of communication with PLCSIM? (My PLCSIM for S7-400 and ET200SP are both in run mode). Thanks in advance. |
Last edited by: Jen_Moderator at: 4/24/2019 9:33:44 AMOptimized link. |
|
4/23/2019 2:24 PM | |
Posts: 76 Rating:
|
UPDATE I have changed some things in the project. Now I don't call GET block in simatic manager, but rather in TIA Portal, so I guess there should not be a problem with "Family" (please read the previous post). Still I get Error = 1 and Status = 1. In the attachment I have provided snapshots of the settings I have done in the project. Hope somebody can help. Attachmentimages.zip (175 Downloads) |
Follow us on