6/12/2009 12:27 PM | |
Posts: 691 Rating:
|
You can go for S7-connection S7-Fault Tolerant will come into picture if you are having 2- CPs in one PC( I think in your case its not there) |
6/12/2009 12:50 PM | |
Posts: 557 Rating:
|
hi find the attachment, which is having a only 1 CP 443-1 having a fault tolerant connection. i think the CP which you are using is having not a fault tolerant faclility. but the connection which i have given in attachment is having a facility. it is allow the generate the fault tolerant connection & the benifit is that whenever any cp will fail it will automaticlly switchover to other cp, but in case of TCP connection it is not possible. regards Attachmentuntitled.zip (115 Downloads) |
6/12/2009 1:41 PM | |
Posts: 163 Rating:
|
Thanku all.Will try and revert back ........... |
6/12/2009 2:02 PM | |
Posts: 163 Rating:
|
CP443-1 used in our project supports fault tolerant connection.Then what is the problem AttachmentCP-FAULT TOLERANT.zip (119 Downloads) |
6/12/2009 11:08 PM | |
Joined: 5/24/2007 Last visit: 4/24/2024 Posts: 284 Rating:
|
Hi Sindhu The problem is what I have been telling all the time. You have no connections coming out from the CP443. I have markedwhere they are missingin your configuration and where it is "Eastern"´s configuration. Krish Attachmentkriscomment.zip (138 Downloads) |
6/13/2009 5:57 AM | |
Posts: 557 Rating:
|
HI I got the problem in your CP, you have not given a MAC address to your PN-IO, after giving a MAC address to your all CP, You will be able to generate the fault tolerant connection.but your MAC address should be different for all four cp.... it will work.... find the attachment.. AttachmentCP.zip (104 Downloads) |
Last edited by: Eastern at: 6/13/2009 6:03 AM |
|
6/16/2009 12:10 PM | |
Posts: 163 Rating:
|
Thanku both.Now it shows no errors. |
6/16/2009 12:40 PM | |
Posts: 163 Rating:
|
What should be connected to LADDR input of AG_LSEND and AG_LRECV since its an S7 fault tolerant connection. Im trying to follow the program in this link https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=18513371&caller=view. Should i call this block(AG_LSEND and AG_LRECV)in the other H station also ? AttachmentLADDR.zip (106 Downloads) |
Follow us on