Industry Online Support
Technical Forum
9/12/2008 2:15 PM | |
Posts: 487 Rating:
|
There are many possibilities. They all use communication blocks. Please see the link below. This has lot of information on communication functions available on S7. http://support.automation.siemens.com/WW/view/en/20982954 Openthe embeded PDF and goto section 2.2.3 which is CPU-CPU communication on profibus. This manual has some table that shows the possibilities between different CPUs and also the data length on different option. This should help you deside which function to use. The manual also has details about each possible communication. The same link also has link to other FAQs with example of each communication. I think this info should help you a lot. Let me know if you need any more help. |
Follow us on