7/2/2015 7:27 AM | |
Posts: 45 Rating: (0) |
hello, I have one problem with communication in Drive Monitor V5.5 SP1 it is the same project, with CP s7400, with IM 467 and CP 443-1 all drives are connected with profibus, my PG/PC communicate with this network on TCP/IP if can help me with some ideas? thanks for the cooperation, best regards, myhay ene ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/2/2015 1:32:26 PMNew subject after splitting |
|