3/27/2018 11:08 AM | |
Posts: 6 Rating:
|
I am facing communication issue of S7 200 Smart PLC with PLC S7-410 Over Profibus Master PLC:: S7410 Slave PLC::S7200 ST60 it is for Water treatment plant supplied by Thermax Communication protocol:: Profibus DP S7200 PROFIBUS CARD: 6ES7 288-7DP01-0AA0 GSD file:: EM DP01 Distance between 2 PLC’s:: 290 meter Baud Rate: 500Kbits/S IO SETTING:: 128 byte IN/Out V area offset:: 4000 Profibus address at both ends are 5 EM DP01 is not detecting by S7410 over profibus network ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 3/27/2018 3:21:21 PMNew subject after splitting |
|
3/27/2018 1:49 PM | |
Posts: 6 Rating:
|
Thanks for reply Please find attached file Profibus address is 5 in S7 HW configuration as well as on EM DP01 port Regards, Pravin Sahane Attachments7200 Communication.zip (516 Downloads) |
3/27/2018 1:51 PM | |
Posts: 6 Rating:
|
Thanks for reply There is no speed setting for profibus in S7 200 side. In S7 400 we set 500Kbits/s Thanks, Regards, Pravin Sahane |
3/29/2018 8:49 AM | |
Posts: 6 Rating:
|
Thanks for reply Please find attached picture of Step7 Configuration for communication with S7200 Please suggest Attachmentwtp S7400.zip (452 Downloads) |
3/29/2018 8:51 AM | |
Posts: 6 Rating:
|
in S7400 Profibus port address of CP443 is 2; and EMDp01 communication GSD for S7200 Profibus address is 5 |
Follow us on