4/10/2019 12:12 PM | |
Joined: 2/12/2017 Last visit: 6/30/2024 Posts: 7 Rating: (0) |
Hello everyone I am using TIA V14 wincc Advance SP1 update 9 in Windows 10 enterprise When I am using simulation between PLC and runtime it was communicate . But when I am taking pc online with PLC ,I can upload download PLC program but communication not established between runtime and PLC , I already check PG/PC interface and Lan setting. Same ip series configure in PLC,Scada,and PC Right now my PC is connected in server network(Company's network). So what things required to communicate my runtime with pLC and existing Network. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/10/2019 2:43:04 PMNew subject after splitting |
|
Follow us on