2/10/2022 4:39 AM | |
Joined: 1/13/2022 Last visit: 2/14/2022 Posts: 3 Rating: (0) |
Is it possible to communicate LOGO! 230RCE with WinCC professional? |
2/10/2022 4:43 AM | |
Joined: 12/18/2014 Last visit: 11/19/2024 Posts: 34239 Rating: (4263)
|
Which WinCC mean you? Classsic or TIA Portal? |
2/10/2022 4:54 AM | |
Joined: 1/13/2022 Last visit: 2/14/2022 Posts: 3 Rating: (0) |
Tia Portal |
2/10/2022 9:30 AM | |
Joined: 12/18/2014 Last visit: 11/19/2024 Posts: 34239 Rating: (4263)
|
The LOGO! 0BA8 (at LOGO!8.1 or higher) can: - Ethernet TCP/IP with the S7 protocol - Modbus TCP/IP |
Follow us on