Industry Online Support
Technical Forum
5/18/2008 8:28 AM | |
Joined: 9/27/2006 Last visit: 7/13/2024 Posts: 12268 Rating:
|
Hello Praven; You will need Com Profibus 5.1 to configure the ET 200U (IM 308C slave) for your S7-300 master. Follow the indications in the following FAQ There is also a downloadable project including a sample Com Profibus file in the link. http://support.automation.siemens.com/WW/view/en/6556876 DP interfacing IM 308-C (slave) and CP 315-2 (master) with STEP 7 V5.2 and COM PROFIBUS V5.1 |
Follow us on