11/28/2015 12:38 PM | |
Joined: 5/20/2015 Last visit: 9/2/2024 Posts: 216 Rating: (3) |
HEY DJ_1 I TOO HAVE A SAME PROBLEM, INFACT I HAVE DEVELOPED AN INTEGRATED PROJECT OF TWO S7-1214C DC/DC/DC CPUs, THING IS THAT THERE IS NO COMMUNICATION AND CONFIGURATION PROBLEM , BUT STILL I AM NOT GETTING OUTPUTS WHEN REQ TO GET OR PUT BLOCKS IT DOES NOT RESPONSE WITH ANY ERROR THATS WHY IT IS DIFFCULT TO DIAGNOSE AND TROUBLESHOOT. MY APPLICATION IS JUST LIKE SYNCRONIASTION BETWEEN TWO DUPLICATE CPUs, AS YOU SAID USE MOVE BLOCK INSTRUCTION TO GET IT DONE. SO PLEASE COULD ANYONE CAN PROVIDE ME A SAMPLE PROGRAM OF SUCH RELEVENT APPLICATION. PLEASE SOMEBODY HELP ME. THANK YOU, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2015 10:09:49 AMNew subject after splitting Let's do it... |
|
11/30/2015 12:09 PM | |
Joined: 5/20/2015 Last visit: 9/2/2024 Posts: 216 Rating: (3) |
HELLO EVERYONE, I HAVE ALMOST DONE WITH ABOVE ISSUE, THING IS THAT I AM NOT GETTING ANY STATUS AT OUTPUT OF GET/PUT BLOCKS, INTERESTING IS THERE IS NO ANY KIND OF ERROR, ON APPLYING POSITIVE EDGE AT REQ TREMINAL. BUT STILL I CAN NOT READ/ WRITE DATA TO REMOTE CPU OF SAME CAT NO. COULD ANYONE RECTIFY MY PROJECT ON THERE PC PLEASE... PLEASE FIND THE ATTACHMENT. AttachmentHT_TIAV13SP1_s71214c_30_11_5pm.zip (753 Downloads) |
Last edited by: gabbar at: 11/30/2015 12:10:55 PMLet's do it... |
|
11/30/2015 12:15 PM | |
Joined: 5/20/2015 Last visit: 9/2/2024 Posts: 216 Rating: (3) |
SOMEBODY HELP ME... IS THERE ANYONE.. PLEASE_ |
Let's do it... |
|
2/10/2016 7:52 AM | |
Joined: 5/20/2015 Last visit: 9/2/2024 Posts: 216 Rating: (3) |
you were Right sandeep |
Let's do it... |
|
9/2/2016 8:48 AM | |
Posts: 1 Rating: (0) |
Hi SanDeep Thank you so much, |
5/25/2018 9:26 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by UHARZA is split to a separate thread with the subject Want to use a PUT instructions with the same IP address Subnet. Best regards |
Follow us on