6/1/2015 3:22 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
NO |
6/2/2015 6:37 PM | |
Joined: 10/3/2013 Last visit: 10/26/2023 Posts: 123 Rating: (3) |
Hi, That means OPC is the open protocol for IT network only not for industrial network right ! THANKS |
6/2/2015 6:58 PM | |
Joined: 9/27/2006 Last visit: 5/24/2024 Posts: 12257 Rating: (2668) |
Hello Mahesh; I feel that your last statement is a rash conclusion. Umencho's answer was a response to your first question, which was based on a misunderstanding of OPC standards. OPC is based on a client/server architecture. An OPC server cannot read/write to an OPC client or an OPC server. Only an OPC client can ask an OPC server for information (read/write). An OPC server can only reply to a request from an OPC client. See the following information from Matrikon, a well-known developper of OPC clients and servers: http://www.matrikonopc.com/resources/opc-server.aspx An OPC Server will respond to requests, and provide data to one or more OPC Clients in a standard, consistent manner. Any compliant OPC Client can interface with, and request data from any compliant OPC Server, regardless of the vendor, or the underlying system providing the data. Please review your initial post, and try to re-write it in terms of OPC basics. Then maybe we can discuss if OPC is a useful standard in automation projects. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/2/2015 8:25:26 PM |
|
1/15/2016 10:38 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by electronicspark1 is split to a separate thread with the subject How can we use the PLC Status/Force control in HMI to show/change user variable I/O, DB?. Best regards |
8/8/2016 12:30 AM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
New question published by Branimir is split to a separate thread with the subject PCS 7 and WINCC OPC server . Best regards |
My Forum is the place to personalize your profile, |
|