7/31/2017 11:33 AM | |
Posts: 648 Rating: (95) |
Dear windberry, please check your commincation settings. Can you take a screenshot for us of your communication settings)? With best regards rh1990 |
8/3/2017 10:23 AM | |
Joined: 8/3/2009 Last visit: 11/6/2024 Posts: 14106 Rating: (1767)
|
Hello I Think it could also be that you use different Profibus parameters in the Classic Project and in the TIA Portal Project with the Panel. You can use a PLC Proxy device to"link" then PLC into the TIA Porject then the Profibus/MPI Parameters will be correct. https://support.industry.siemens.com/cs/de/en/view/73502293 Bye Murof EDIT: Or do you work with one TIA Project with all devices ?? |
Last edited by: Murof at: 8/3/2017 10:24:40 AMIf this Information really helps, you could use the Rate function |
|
Follow us on