4/14/2020 10:54 AM | |
Joined: 12/29/2008 Last visit: 4/18/2024 Posts: 5 Rating: (0) |
Dear all, It has been for some time now that I can't connect to a CPU over the ethernet network with my laptop. I can connect to the CP but not to the CPU. Only, when I remove the HMI (TP177B) from the network, I can connect again. That seems easy, It must be a problem with connection resources but it looks like there are enough resources available. See attachment. There are two S7 connections with another CPU and one with a SCADA system. Maybe I overlooked something but I am now at a point where I would replace the CPU. Before I do that however, I would like to have your opinions. Best regards, AttachmentComm report PLC HD.docx (60 Downloads) |