5/31/2014 7:08 PM | |
Joined: 12/1/2012 Last visit: 7/30/2024 Posts: 128 Rating: (4) |
Yes on ping it shows send receive |
6/1/2014 5:15 AM | |
Posts: 691 Rating: (36) |
Please Check the System Parameters in the WinCC |
This contribution was helpful to1 thankful Users |
6/1/2014 2:44 PM | |
Posts: 510 Rating: (117) |
In "Setting the PGPC Interface", is the "CP-TCPIP" linked to the Ethernet card of the PC Station? Regards, billwest |
6/1/2014 9:46 PM | |
Posts: 114 Rating: (12) |
check anti virus protction and scan ur pc once then made protection off then check
|
Follow us on